PD-I
Original operating instructions
Information about the documentation
About this documentation
- Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
- Observe the safety instructions and warnings in this documentation and on the product.
- Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
Explanation of symbols used
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the documentation
The following symbols are used in this document:![]() |
Read the operating instructions before use. |
![]() |
Instructions for use and other useful information |
![]() |
Dealing with recyclable materials |
![]() |
Do not dispose of electric equipment and batteries as household waste |
Symbols in the illustrations
The following symbols are used in illustrations:![]() |
These numbers refer to the corresponding illustrations found at the beginning of these operating instructions |
![]() |
The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text |
![]() |
Item reference numbers are used in the overview illustrations and refer to the numbers used in the product overview section |
![]() |
This symbol is intended to draw special attention to certain points when handling the product. |
Product-dependent symbols
Symbols on the product
The following symbols can be used on the product:![]() |
Read the operating instructions. |
Button symbols
The buttons on the product are as follows:![]() |
Distance button |
![]() |
Functions button |
![]() |
Add button |
![]() |
Subtract button |
![]() |
Bluetooth button |
![]() |
Memory | Timer button |
![]() |
Reference button |
![]() |
On | Delete | Off button |
Display icons (functions)
The icons that can appear on the product's display are as follows:![]() |
Measuring area |
![]() |
Measure volumes |
![]() |
Pythagoras (2-point) |
![]() |
Pythagoras (3-point) |
![]() |
Layout function |
Display icons (general symbols)
The icons that can appear on the product's display are as follows:![]() |
Battery state of charge |
![]() |
Bluetooth |
![]() |
Add distances |
![]() |
Subtract distances |
![]() |
Reference |
![]() |
Timer |
![]() |
Data storage |
Declaration of conformity
We declare, on our sole responsibility, that the product described here complies with the applicable directives and standards. A copy of the declaration of conformity can be found at the end of this documentation.The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | 86916 Kaufering, Germany
Product information
![Image alternative](https://files-techDocs.hilti.com/2222190/H2_SYM-Logo_M_M_DEU_Hilti-Logo.jpg)
There is a label bearing the serial number on the bottom of the battery compartment.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
Product informationLaser range meter PD-I Generation 02 Serial no.
Laser information on the product
Designation and explanation![]() |
Class 2 laser. Do not stare into the beam. Do not direct the beam toward other persons or toward areas in which other persons, who are not involved in the work with lasers, may be present. |
Laser classification for Class 2 laser products
The device complies with Laser Class 2 in accordance with IEC 60825-1:2014 /EN 60825-1:2014. These devices can be used without further protective measures.Data for classification
Wavelength |
620 nm … 690 nm |
Maximum radiant output power for classification |
≤ 1 mW |
Pulse duration |
≥ 400 |
Pulse repetition frequency |
320 MHz |
Beam divergence |
0.16 mrad x 0.6 mrad |
Safety
Safety instructions
General safety measures
- Check the product for damage before use. Have damage repaired by Hilti Service.
- Check the accuracy of the product if it has been dropped or subjected to other mechanical stresses.
- Although the product is designed for the tough conditions of jobsite use, like other measuring instruments it should be treated with care.
- When not in use, products must be stored in a dry, high place or locked away out of reach of children.
- The product is not intended for use by children.
- Comply with national health and safety requirements.
Basic safety precautions
In addition to the information relevant to safety given in each of the sections of these operating instructions, the following points must be strictly observed at all times. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.- Keep all safety instructions and other instructions for future reference.
- Stay alert, watch what you are doing and use common sense when operating the product. Do not use the product while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating the product can result in serious personal injury.
- Do not render safety devices ineffective and do not remove information and warning notices.
- Laser radiation in excess of Class 2 can be emitted if the product is opened without correct procedure being followed. Have the product repaired by Hilti Service only.
- Do not tamper with or attempt to make alterations to the product.
- Before starting to use the product, always make sure that it is full working order.
- Readings taken through panes of glass or similar materials can falsify the result of measurement.
- People passing through the laser beam or other quick changes in measuring conditions can falsify the result of measurement.
- Never aim the product against the sun or other powerful light sources.
- Take the influences of the surrounding area into account. Do not use the device where there is a risk of fire or explosion.
- Follow the directions for operation, care and maintenance in the operating instructions.
Working safely with laser tools
- Laser Class 2/Class II tools may be operated only by appropriately trained persons.
- Laser beams should not be projected at eye height.
- Precautions must be taken to ensure that the laser beam does not unintentionally strike highly reflective surfaces.
- Precautions must be taken to ensure that persons do not stare directly into the beam.
- The laser beam must not be allowed to project beyond the controlled area.
- Switch the laser tool off when it is not in use.
- Store laser tools, when not in use, in places to which unauthorized persons have no access.
Proper arrangement of the workplace
- Avoid unusual postures when working on ladders. Maintain firm footing and balance at all times.
- Secure the site where you are taking measurements and when using the product do not direct the laser beam toward other persons or toward yourself.
- When the product is brought into a warm environment from very cold conditions, or vice-versa, allow it to become acclimatized before use.
- Use the product only within its specified limits.
- Keep the laser aperture clean to avoid measurement errors.
- Comply with the national accident prevention regulations.
Electromagnetic compatibility
Although the product complies with the strict requirements of the applicable directives, Hilti cannot entirely rule out the possibility of interference to the product caused by powerful electromagnetic radiation, possibly leading to incorrect operation. Check the accuracy of the device by taking measurements by other means when working under such conditions, or if you are unsure. Likewise, Hilti cannot rule out the possibility of interference with other devices (e.g. aircraft navigation equipment). The product complies with the requirements of class A; the possibility of interference in a residential environment cannot be excluded.Only for Korea: This laser range meter is suitable for commercial and industrial use and for the electromagnetic radiation encountered in this field (Class A). The user must be aware of this and shall not use this laser range meter in residential environments.
Description
Product overview
![Image alternative](https://files-techDocs.hilti.com/2222190/H2_BILD-Objekt_System_PD_I-G2_DEU_PD-I_UEBERSICHT.png)
- Display
- Distance button
- Functions button
- Bluetooth button
- Memory | Timer button
- On | Delete | Off button
- Reference button
- Subtract button
- Add button
- Spike
- Battery-compartment cover
Intended use
The product described is a laser range meter. It is designed for single measurements and for continuous measurement of distances.
Distances can be measured to any stationary target, i.e. concrete, stone, wood, plastic, paper, etc. The use of prisms or other highly reflective targets is not permitted and can falsify the results.The product is approved for use with batteries of type AAA.
Bluetooth®
This product has Bluetooth.Bluetooth is a wireless data transfer with which two Bluetooth-enabled devices can communicate with each other over a short distance.
Hilti products ship ex-works with Bluetooth deactivated.
Switching Bluetooth on or offPress the
![Image alternative](https://files-techDocs.hilti.com/2222190/H2_SYM-Icon_System_PD_I-G2_DEU_PDI_TASTE_05.jpg)
Items supplied
Laser range meter, belt pouch, wrist strap, 2x AAA battery (1.5 V), "Quick Start" guide, safety instructions, manufacturer's certificate, declaration of conformityTechnical data
Product properties
Dimensions (L x W x H) |
125 mm x 46 mm x 26 mm |
Weight (including batteries) |
111 g |
Length (spike) |
65 mm |
Smallest displayed unit |
0.1 mm |
Protection class in accordance with IEC 60529 |
IP 54 |
Operating temperature |
−10 ℃ … 50 ℃ |
Storage temperature |
−25 ℃ … 70 ℃ |
Laser properties
Laser type |
635 nm | < 1 mW |
Laser class in accordance with EN 60825-1:2014 |
Laser class 2 |
Range (ideal conditions) |
0.05 m … 100 m |
Accuracy (ideal conditions) ± |
1.5 mm |
Battery time
Battery time (measurements) |
≈ 10,000 |
Automatic switch-off (laser) |
after 90 seconds |
Automatic switch-off (product) |
after 180 seconds |
Bluetooth Smart
Version |
v4.0 |
Range |
< 10 m |
Before use
Inserting the batteries
![Image alternative](https://files-techDocs.hilti.com/2222190/H2_BILD-Objekt_System_PD_I-G2_DEU_PD-I_010.jpg)
- Flip the contact spike forward.
- Open the battery compartment.
- Insert the batteries.
- Close the battery compartment and flip the contact spike back to the closed position.
Switching the laser range meter on or off
- Press the
button to switch the laser range meter on.
- Press the
button and hold it down for 2 seconds to switch the laser range meter off.
Undo
- Take a measurement.
- Press the
button.
- The last measurement is undone.
- The last measurement is undone.
Basic settings
Setting the reference
- Press the
button and hold it down for 2 seconds to toggle the reference setting.
- The reference is changed.
- The reference is changed.
Setting the unit of measure
The unit of measure cycles through the following:![Image alternative](https://files-techDocs.hilti.com/2222190/H2_BILD-Objekt_System_PD_I-G2_DEU_PD-I_020.jpg)
- Simultaneously press the
and
buttons and hold them down for 2 seconds.
- The unit of measure is changed.
- The unit of measure is changed.
- Repeat step 1 until the unit of measure you want is set.
Switching the acoustic signal on or off
- Simultaneously press the
and
buttons and hold them down for 2 seconds.
Using the contact spike
![Image alternative](https://files-techDocs.hilti.com/2222190/H2_BILD-Objekt_System_PD_I-G2_DEU_PD-I_030.jpg)
- Flip the contact spike open through 90°.
- The contact spike can be used as an end stop.
- The contact spike can be used as an end stop.
- Flip the contact spike open through 180°.
- The reference is changed automatically.
- The reference is changed automatically.
Measuring using a target plate
Use the target plate to measure distance under the following unfavorable conditions:- The wall is not sufficiently reflective due to the type of surface.
- The target point is not on a surface.
- The distance to be measured is too long.
- The light conditions are unfavorable (bright sunshine).
Operation
Overview of the functions
Press the![Image alternative](https://files-techDocs.hilti.com/2222190/H2_SYM-Icon_System_PD_I-G2_DEU_PDI_TASTE_02.jpg)
![Image alternative](https://files-techDocs.hilti.com/2222190/H2_BILD-Objekt_System_PD_I-G2_DEU_PD-I_050.jpg)
Main functions
Measure distance (single measurement)
- Aim the laser at a target point.
- Press the
button.
- Measurement has been completed.
- Measurement has been completed.
- For more single measurements, switch the laser on and repeat the procedure.
Measuring area
![Image alternative](https://files-techDocs.hilti.com/2222190/H2_BILD-Objekt_System_PD_I-G2_DEU_PD-I_060.jpg)
- Aim the laser at a target point for the room length.
- Press the
button.
- Aim the laser at a target point for the room width.
- Press the
button.
- Measurement has been completed.
- Measurement has been completed.
Measuring wall areas (decorator function)
![Image alternative](https://files-techDocs.hilti.com/2222190/H2_BILD-Objekt_System_PD_I-G2_DEU_PD-I_110.jpg)
- Aim the laser at a target point for the room length.
- Press the
button.
- The initial value appears in the top row.
- The initial value appears in the top row.
- Add or subtract measured values.
- Repeat steps 1 to 3 until you have measured all the wall lengths.
- Aim the laser at a target point for the room height.
- Press the
button.
- Measurement has been completed.
- Measurement has been completed.
Measuring volume
![Image alternative](https://files-techDocs.hilti.com/2222190/H2_BILD-Objekt_System_PD_I-G2_DEU_PD-I_070.jpg)
- Aim the laser at a target point for the room length.
- Press the
button.
- Aim the laser at a target point for the room width.
- Press the
button.
- Aim the laser at a target point for the room height.
- Press the
button.
- Measurement has been completed.
- Measurement has been completed.
Measure Pythagoras (2-point)
![Image alternative](https://files-techDocs.hilti.com/2222190/H2_BILD-Objekt_System_PD_I-G2_DEU_PD-I_080.jpg)
- Aim the laser at the first target point.
- Press the
button.
- Aim the laser as the second target point at right angles to the target distance.
- Press the
button.
- Measurement has been completed.
- Measurement has been completed.
Measure Pythagoras (3-point)
![Image alternative](https://files-techDocs.hilti.com/2222190/H2_BILD-Objekt_System_PD_I-G2_DEU_PD-I_090.jpg)
- Aim the laser at the first target point.
- Press the
button.
- Aim the laser as the second target point at right angles to the target distance.
- Press the
button.
- Aim the laser at the third target point.
- Press the
button.
- Measurement has been completed.
- Measurement has been completed.
Using the Layout function
![Image alternative](https://files-techDocs.hilti.com/2222190/H2_BILD-Objekt_System_PD_I-G2_DEU_PD-I_100.jpg)
- Use the
and
buttons to set the distance between the layout points.
- Press the
button to confirm the value.
- Take the measurement by passing the laser range meter along the layout baseline.
- Press the
button to end measurement.
Special functions
Adding or subtracting measurements
You can use the "Add/Subtract" function to add or subtract the measured values of different functions.- Use one of the compatible functions.
- Press the
button if you want to add a new measured value or press the
button if you want to subtract.
- Take another measurement.
Retrieving or deleting data from data memory
- Press the
button.
- The 10 most recent measured values are displayed.
- The 10 most recent measured values are displayed.
- Use the
or
buttons to browse through the measured values in memory.
- Simultaneously press the
and
buttons and hold them down for 2 seconds to delete the measured values saved in the device's data memory.
- All measured values are deleted from the device's data memory.
- All measured values are deleted from the device's data memory.
Taking a continuous measurement (min/max)
- Press the
button and hold it down for 2 seconds to start measuring.
- Press the
button to stop measuring.
Taking delayed measurement (timer function)
- Press the
button and hold it down for 2 seconds.
- Use the
and
buttons to set the timer.
- Press the
button to confirm the value.
- The countdown starts.
- The countdown starts.
Using Bluetooth Smart
- Press the
button and hold it down for 2 seconds to switch Bluetooth on.
- Establish a connection between the mobile device and the laser range meter.
Fault codes
Press the![Image alternative](https://files-techDocs.hilti.com/2222190/H2_SYM-Icon_System_PD_I-G2_DEU_PDI_TASTE_01.jpg)
![Image alternative](https://files-techDocs.hilti.com/2222190/H2_SYM-Icon_System_PD_I-G2_DEU_PDI_TASTE_08.jpg)
Malfunction |
Possible cause |
Action to be taken |
---|---|---|
204 |
Calculation error |
|
220 |
General hardware fault. |
|
240 |
Fault in data transmission |
|
252 |
Product has overheated. |
|
253 |
The product is too cold. |
|
255 |
Incoming signal too weak, measurement takes too long. |
|
256 |
Incoming signal too high |
|
257 |
Target surface too bright |
|
trc |
Distance was less than the minimum measurable distance. |
|
Distance was greater than the maximum measurable distance. |
|
Care, transport and storage
Cleaning
- Do not touch the lens with the fingers.
- Clean the lens by blowing off dust or by wiping with a clean, soft cloth.
- Use only pure alcohol or water for cleaning.
- Do not dip the laser range meter into water.
Transport
- Use the Hilti packaging or packaging of equivalent quality for transporting or shipping your equipment.
Storage and drying
- Do not put the product into storage when wet. Allow it to dry before putting it away.
- Observe the temperature limits given in the Technical Data section which are applicable to storage or transport of the equipment.
- Check the accuracy of the equipment before it is used after a long period of storage or transportation.
Disposal
![Image alternative](https://files-techDocs.hilti.com/2222190/H2_SYM-Hinweis_M_M_DEU_Recycling_f.jpg)
In accordance with the European Directive on waste electrical and electronic equipment and its implementation in conformance with national law, electric tools or appliances that have reached the end of their life must be collected separately and returned to an environmentally compatible recycling facility.
RoHS (Restriction of Hazardous Substances)
Click on the link to go to the table of hazardous substances: qr.hilti.com/r9121031.There is a link to the RoHS table, in the form of a QR code, at the end of this document.
Japanese Radio Law compliance
This device is granted persuant to the Japanese Radio Law (電波法).Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.
![Image alternative](https://files-techDocs.hilti.com/2222190/H2_BILD-Objekt_System_PD_I-G2_DEU_Konform.jpg)
![Image alternative](https://files-techDocs.hilti.com/2222190/H2_BILD-Objekt_System_PD_I-G2_DEU_QR_PD-I_r9121031.jpg)